ST-LINK/V2 jtag/SWD probe fails to connect to the STM32 Micro
Hi everybody, please help if you know the answer.
I have the following Micro and tools and unfortunately I am not able to debug the micro.
STM32F439 MCU on a board (this is not a development board though)
System Workbench for STM32
IDE // ST-LINK/V2 jatg probe fails to connect
STM32 ST-LINK Utility
tool
// ST-LINK/V2 jtag probe
connects and I can program the Micro
note: NRST pin of the micro is not connected to NRST pin on the ST-LINK probe.
I can connect and program the micro using the above utility tool.
but I can not connect to the micro using the above IDE and it fails, the debugger console gives me the following message:
Info : device id = 0x20016419
Info : flash size = 2048kbytesInfo : Stlink adapter speed set to 1125 kHzadapter speed: 1125 kHzError: timed out while waiting for target haltedTARGET: STM32F439NIHx.cpu - Not haltedin procedure 'reset' in procedure 'ocd_bouncer'Info : Stlink adapter speed set to 1125 kHzadapter speed: 1125 kHzError: timed out while waiting for target haltedTARGET: STM32F439NIHx.cpu - Not haltedin procedure 'reset' in procedure 'ocd_bouncer'Error: Target not halted
Error: failed erasing sectors 0 to 5Error: flash_erase returned -304shutdown command invoked#stm32