Skip to main content
N. SANTINI
ST Employee
September 4, 2019

FAQ: GUI on STM32F469-Discovery boards using CubeMX and STemWin

  • September 4, 2019
  • 1 reply
  • 16168 views
How to build a GUI application for the STM32F469-Discovery board using the STemWin Graphical library and starting from the CubeMX tool default configuration.

When selecting an ST development board such as the STM32F469-Discovery one some default settings are suggested (i.e. some peripherals are enabled and configured).
If all the peripherals required for a GUI (Graphical User Interface) are then enabled their configuration need some adaptation, moreover some useless peripherals, as far as a GUI application is concerned, are also enabled.
Finally the generated code also needs to be updated to cope with some known limitation in CubeMX. 
This article will guide the customer with these 3 steps:

  1. disable not needed peripherals
  2. adapt configuration of required ones
  3. fix the generated source code

This tutorial applies to CubeMX 5.3.0, notably step 3 maybe become unnecessary in future versions.
The following steps are divided into 2 sections, the first one is common to all IDEs.
For Atollic, AC6 System Workbench and CubeIDE you may also follow the second section steps.

1. All IDEs

1.1. Launch CubeMX and select the STM32F469-Discovery from the Board Selector list, then click on "Start Project"

Note : For CubeIDE, follow the same steps but launching the CubeMX from CubeIDE instead, interface is identical.
 
103.png

1.2. Agree to initialize peripherals to their default settings clicking "Yes" in the dialog box

104.png

1.3. Change the peripherals list to A->Z filtering

105.png

1.4. Start disabling some useless (for a GUI application perspective) peripherals 

FATFS : uncheck "SD Card"
I2C1 : set to "Disable"
I2C2 : set to "Disable"
SAI1 : Set SAI A mode to "Disable"
SDIO : Set mode to "Disable"
USART3 : Set mode to "Disable"
USART6 : Set mode to "Disable"
USBHOST : Set Class for FS IP to "Disable"
USB_OTG_FS : Set Mode to "Disable"

1.5. Update the configuration of some peripherals

LTDC - Mode : set Display Type to "RGB565 (16 bits) - DSI mode"
LTDC - Configuration - Parameter Settings : set Active Width to 400
LTDC - Configuration - Layer Settings : set Layer 0 Window Horizontal Stop to 400
LTDC - Configuration - Layer Settings : set Layer 0 Color Frame Buffer Line Length to 400
DSIHOST - Configuration - Display Interface : set Maximum Command Size to 400
GRAPHICS - Mode - Graphics Framework : select "STemWin"
GRAPHICS - Mode - Display Interface : select "Display Serial Interface using LTDC-DSIHOST"
GRAPHICS - Configuration - Parameter Settings: set "User GUIBuilder Tool" to "Enable"
GRAPHICS - Configuration - Parameter Settings: set Physical Display Size - X Size to "800"
GRAPHICS - Configuration - Platform Settings: select PH7 as LCD Reset Pin

1.6. Select your IDE from the list in the Project Manager -> Project section

106.png

1.7. Generate the code once

107.png

1.8. Go back to pinout & Configuration then in the GRAPHICS peripheral
In the Configuration launch GUIBuilder by clicking Execute

108.png

1.9. In GUIBuilder let's just add a buttton

109.png

1.10. Select "File->Save", agree to overwrite existing file

110.png

1.11. Close GUIBuilder and generate the code again 

111.png


2. Code editing

HW_Init.c needs to be updated manually, depending on the chosen IDE this file is either in a target folder or in the src one.
Update needed:
Replace OTM8009A_ORIENTATION_PORTRAIT by OTM8009A_ORIENTATION_LANDSCAPE in OTM8009A_Init call :
112.png
Explanation
The DSI display present on this discovery board has a specificity that forces to split its refresh into 2 steps to avoid flickering.
So as far as LTDC and DSI are concerned the width of the display is set to 400 instead of 800.
Unfortunately the parameter specifying the display orientation that will be transferred to the display low-level driver is based on the ratio between width and height extracted from LTDC configuration.
In this case width is smaller than height so PORTRAIT mode is selected and LANDSCAPE is greyed-out :
113.png
that is why the modification must be done directly in the source code and must be done again each time the code is re-generated from the CubeMX.


3. Eclipse-based IDEs (Atollic, AC6 System Workbench, CubeIDE)

For these IDEs the source code corresponding to reset pin configured in CubeMX is not properly generated and has to done manually.
Open Stemwin_wrapper.c file, look for the LCD_LL_Reset(void) function declaration and replace it by:

static void LCD_LL_Reset(void)
{
   /* Activate XRES active low */
   HAL_GPIO_WritePin(GPIOH, GPIO_PIN_7, GPIO_PIN_RESET);
   HAL_Delay(20); /* wait 20 ms */
   /* Desactivate XRES */
   HAL_GPIO_WritePin(GPIOH, GPIO_PIN_7, GPIO_PIN_SET);
   /* Wait for 10ms after releasing XRES before sending commands */
   HAL_Delay(10);
}

Then in the GRAPHICS_HW_Init() function, call the function :

void GRAPHICS_HW_Init(void)

  MX_FMC_Init();
  MX_SDRAM_InitEx();
  /* USER CODE BEGIN LCD_reset_pin */
  LCD_LL_Reset();
  /* USER CODE END LCD_reset_pin */

  MX_LCD_Init();      /* LTDC struc, layer struct */
  MX_DMA2D_Init();
  DMA2D_Init();
  MX_DSI_Init();
}


This is the end of this tutorial, I hope it will be helpful.
 


 

This topic has been closed for replies.

1 reply

Associate II
September 13, 2023

I suppose this was create before touchGFX?