Hi @BXie.1 welcome to ST Community.
The X-NUCLEO-IHM03A1 is based on powerSTEP01 System-In-Package able to manage up to 10 Arms.
This device and the board can operate with both voltage mode driving and advanced current control, more setting are needed according the selected working mode.
In case of voltage mode, the sense resistors are not required and you can remove them connecting the SENSE pins directly to ground.
In case of current mode you have to select the proper value of sensing resistor and reference voltage according to your target current.
The mounted value is selected to work with a few ampere (with power dissipation margin on sense resistors).
"If you feel a post has answered your question, please click ""Accept as Solution"""