Skip to main content
Andrew Lohmann
Senior
Mar 25, 2021 5:33 PM UTC
Solved

Will all or any battery charger ICs operate properly with rectified AC input?

Will all or any battery charger ICs such as L6924U operate properly with rectified AC input?

The rough circuit below is of a bicycle dynamo that delivers 300mA-500mA of varying AC frequency and current ripple will this prevent the charger controller from working properly?

https://photos.app.goo.gl/7W1iKxkfDLhZqULw6

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Apr 6, 2021 7:00 AM UTC

    In principle, nothing speaks against operating the L6924U or L6924D in this way.

    However, you must pay attention to the maximum input voltage of 16V, since bicycle dynamos are more power current sources than voltage sources and can generate very high voltages when running without or very small load.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Apr 6, 2021 7:00 AM UTC

    In principle, nothing speaks against operating the L6924U or L6924D in this way.

    However, you must pay attention to the maximum input voltage of 16V, since bicycle dynamos are more power current sources than voltage sources and can generate very high voltages when running without or very small load.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Andrew Lohmann
    Senior
    Apr 6, 2021 7:17 AM UTC

    Thanks possibly the circuit is not visible but it does have voltage limiting that you advise. I suspect the your answer will be true of many similar ICs including others made by other manufacturers but the detail is not clear.

    Peter BENSCH
    ST Technical Moderator
    Apr 6, 2021 8:03 AM UTC

    The voltage limiter with a crowbar is clearly visible - but it takes a TRIAC some time to fire. The max rating of 16V is the absolute maximum, i.e. even short-term and slight exceeding can damage the device. You could consider adding a TVS diode behind the Schottky full bridge rectifier, e.g. the SMBJ13A.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.