Skip to main content
TRose.6
Visitor II
June 2, 2023
Question

Why would I use a STM704 instead of a STM806 battery monitor?

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    June 5, 2023

    Welcome, @Terry Rose​, to the community!

    The differences between STM704 and STM806 are indeed not listed on the first page of the data sheet, but can be found after a close look at the parameter tables:

    • VPFI (Power-fail comparator, data sheet, pg. 33)
      • STM704: 1.237V±2%
      • STM806: 1.237V±4%
    • VRST (Reset thresholds, data sheet, pg. 34)

    So to answer your question, the cheaper STM806 is the one to use if you have lower accuracy requirements.

    Hope that helps?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.