Skip to main content
Ksun.12
Visitor II
December 16, 2020
Question

Why motor vibration in zero speed? i'm using G431B board T-MOTOR 2312 and hall sensor(120 degree), set to torque mode, the motor work fine most time, but it will be vibration when start-up with heavy load or i stop the motor with my hand.

  • December 16, 2020
  • 0 replies
  • 614 views

Hi guys,

How can i solve the problem that motor vibration in zero speed? i'm using G431B board T-MOTOR 2312 and hall sensor(120 degree), set to torque mode, the motor work fine most time, but it will be vibration when start-up with heavy load or i stop the motor with my hand. 

Is that normal? i did not see this problem in other foc drivers like VESC​ or odrive.

​

Really appreciated for any help.

This topic has been closed for replies.