Skip to main content
Electric Forest
Associate II
September 23, 2018
Question

Why is torque falling at low speed?

  • September 23, 2018
  • 4 replies
  • 1316 views

I'm running the motor in torque mode with an encoder. It works really well.

The only problem I have is that something internal to the FOC software adjusts the torque down at (very) low and zero speed. I assume this is done to avoid the motor overheating.

Example:

I align and start the motor, it quickly spins up and draws 20W. Lots of torque.

I apply some friction to the motor and it still draws approx 20W.

I apply more and more friction, the speed falls as I apply more friction. At some point when the speed gets low the power draw gradually falls.

I force the motor to a complete stop, the power draw is almost zero. Almost zero torque obviously.

I let go of the motor, it spins up again and draws 20W.

So my questions are pretty simple:

- What is affecting my torque at low/zero speeds?

- How do I increase torque at low/zero speeds?

Any pointers are greatly appreciated.

This topic has been closed for replies.

4 replies

Mark-S
Associate II
September 24, 2018

Hello, I am having the same issue. Did you resolve this issue? If so, how?

Electric Forest
Associate II
September 24, 2018

No, I won't have time to look at this for a few days. But I've sort of given up, I've looked at all the source code without finding this.

Mark-S
Associate II
September 24, 2018

Thanks for your feedback.

Electric Forest
Associate II
October 1, 2018

I'm still wondering about this. Anyone knows if this is expected behaviour? And, ideally, how do I change it?