Skip to main content
cliang
Associate II
April 22, 2015
Question

Why does L6480H driver register value reset to default

  • April 22, 2015
  • 3 replies
  • 838 views
Posted on April 22, 2015 at 19:07

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This topic has been closed for replies.

3 replies

cliang
cliangAuthor
Associate II
April 23, 2015
Posted on April 23, 2015 at 15:06

the chip wont reset if I send GetParam or GetStatus command. As long as the command is motion command, it will reset. I call it reset because register value suddenly reset to default value. I know reset the chip by pull Reset pin low or power cycle. However, it did not get either power cycle or reset.

Please help. 

Enrico Poli
ST Employee
April 27, 2015
Posted on April 27, 2015 at 10:02

Hi,

The device could be reset by a drop of the supply voltage. Maybe when you try to turn on the motor the power supply does not keep the voltage stable.

Please, check all the supply pins of the IC (VREG, VCC and VSREG)

Regards

Enrico

cliang
cliangAuthor
Associate II
April 27, 2015
Posted on April 27, 2015 at 15:20

Thanks. found the issue.