Skip to main content
Anton Lloves
Visitor II
June 25, 2018
Question

Why an extra resistor on EV-VNH7040AY motor controller evaluation board?

  • June 25, 2018
  • 0 replies
  • 610 views
Posted on June 25, 2018 at 16:25

Hello all,

I have a question regarding the EV-VNH7040AY DC motor controller evaluation board. In the package it is included with the board a 1K

?

resistor that I have no idea what it is for. My guess is that is has to do maybe with the current mirroring feature but I am not sure since I am a newbe in the field of motor control electronics.

Can somebody clarify what is the use of this extra included in the package?

Thank you

#evaluation-board #res #motor-dc #why-resistor #ev-vnh7040ay-resistor-why-evaluation-board-motor-dc #resistor #dc-motor-control
This topic has been closed for replies.