Skip to main content
EBaye.1
Visitor II
Nov 24, 2021 3:28 PM UTC
Question

Why 400V 800W PFC with L4984D function ok when the load is resistive but not when the load is a switching with a transformer?

Hello, I designed and manufactured a PFC circuit with a L4984D for 400V 800W output. I tested it until 860W with a resistive load and function ok. I need to power with it a 600W, 400V to 24V DCDC. This second step consist of a full bridge with a transformer (Lp=1.3mH, Lleak=5uH, Rp=100mohm), when I tested it without final load the PFC achieves 400V, but when I connect a minimal load (50W) it falls down to 360V, up to 320V with more power output. can someone help me to solve this problem?

    This topic has been closed for replies.