Skip to main content
HPawa.1
Visitor II
December 19, 2019
Question

Which is the best suitable isolated flyback controller for the input upto 1KVDC and output of 20W ?

  • December 19, 2019
  • 0 replies
  • 514 views

I am designing a Isolated Flyback SMPS with input range upto 1KV and output of 20W. I couldn't found any flyback controller which will support this range.

I found one offline PWM controller named STCH03 which is having limited 650V start-up.

So is it possible to extend the HV pin range of this controller upto 1KV by adding series resistors ?

Or is there any better controller that I can start working with ?

This topic has been closed for replies.