Skip to main content
JWagn.3
Visitor II
March 22, 2023
Question

Where could i find the Firmware for EV-SPC582B to operate the EV-VNF1048F via the STSW-EV-VNF1048F is the graphical user interface (GUI). No information in the User manual

Extract from your user manual:

Introduction

The STSW-EV-VNF1048F is the graphical user interface (GUI) dedicated to set and control the EV-VNF1048F using an EVSPC582B programmed with a specific firmware able to create an advanced controller for a MOSFET in high side configuration, designed for the implementation of an intelligent high side switch for 12 V, 24 V and 48 V automotive applications.

    This topic has been closed for replies.

    1 reply

    Visitor II
    September 30, 2024

    I have the same problem. Can not find the "dedicated software" for the Eval board. I wonder why they choose that expensive EVSPC582B board instead of using a cheaper and more convenient Nucleo board with STM32?

    It would be much simpler if they provide a SPI Library for the VNF1048F.