Skip to main content
daded.1
Associate II
December 30, 2021
Solved

What is the nest best replacement for the STPMIC1APQR?

I would like to start a project with the STM32MP157D microprocessor but cant find the power management chip due to supply issues and I do not know any suitable replacement.

Thanks!

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
January 7, 2022

Hi @daded.1​ ,

Maybe your prototyping could be done using STM32MP157D-DK1 or STM32MP157D-EV1 board (on EV1, is it possible to use the daughter board alone).

Alternatively, you could probably find suitable modules using STM32MP157D on 3rd party vendors (e.g. partners, but not limited to).

Otherwise, it is possible to use the STM32MP1 without STPMIC1. Some low power modes will not be available. Please refer to AN5031 and AN5256.

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

4 replies

Peter BENSCH
ST Technical Moderator
December 30, 2021
As you can see from the datasheet, the STPMIC1 is available in several options:
The STPMIC1A, STPMIC1B, STPMIC1D and STPMIC1E are pre-programmed devices to support the STM32MP1 series application processor versions.
The STPMIC1C is not a programmed device to support custom applications
Although pre-programmed, versions A, B, D and E can also be reprogrammed to any other value.
Good luck!
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
daded.1
daded.1Author
Associate II
December 30, 2021

Thanks for the response @Peter BENSCH​ 

My challenge is that none of those variants are available for order, and the lead times are just to faraway considering this will be used to learn and prototype.

Is there any other device that can be used or will it be possible to prototype with the STM32MP157D microprocessor without using the STPMIC1?

PatrickF
PatrickFBest answer
ST Employee
January 7, 2022

Hi @daded.1​ ,

Maybe your prototyping could be done using STM32MP157D-DK1 or STM32MP157D-EV1 board (on EV1, is it possible to use the daughter board alone).

Alternatively, you could probably find suitable modules using STM32MP157D on 3rd party vendors (e.g. partners, but not limited to).

Otherwise, it is possible to use the STM32MP1 without STPMIC1. Some low power modes will not be available. Please refer to AN5031 and AN5256.

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
JDave.4
Associate III
January 26, 2022

Same problem.... We have a custom board but we are unable to find the STPMIC1A in stock. The MPU is available but no PMIC. Why doesn't ST provide sample stock? We need a few pcs for prototyping.