Skip to main content
Arju
Visitor II
June 15, 2020
Question

What is the maximum switching frequency of PWD13F60?

  • June 15, 2020
  • 1 reply
  • 512 views

..

This topic has been closed for replies.

1 reply

Cristiana SCARAMEL
ST Employee
June 16, 2020

​The maximum switching frequency depends on application requirements, for example from the high voltage bus value, load current, load type and switching method (hard- or soft-switching).

Primarly, the switching frequency is limited by the switching losses (heat dissipation). You can estimate the maximum frequency, using your application requirements and the MOSFET characteristics reported in the PWD13F60 datasheet at page 10.

"If you feel a post has answered your question, please click ""Accept as Solution"""