The dies inside are identical, but the internal connection is a bit different. This means that apart from the maximum total power dissipation, the electrical parameters are completely identical.
The thermal resistance Rthj-lead increased from 15K/W (VNS1NV04D-E) to 30K/W (VNS1NV04DP-E), so the absolute maximum total power dissipation decreased from 8.3W to 4W, which must be taken into account for the cooling measures.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.