Skip to main content
Visitor II
November 27, 2023
Question

What is the difference between the LM211 and LM311

The datasheet says that 

LM211D/DT has a temperature of -40 °C, +105 °C and output to negative supply voltage 50V

LM311D/DT has a temperature of -0 °C, +70 °C and output to negative supply voltage 40V

Is there any differences in performance or electrical characteristics between the two?

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
November 27, 2023

Welcome @jgananam, to the community!

No, there are no differences in performance.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.