Question
What happens to VND5T050AK-E CSn output when you overload the output?
Posted on March 30, 2016 at 10:29
We need to settle a difference of opinion interpreting the data sheet for the VND5T050AK-E, dual channel high-side driver IC.
We agree that when you provide a normal load, the CSn output acts as a current source whose current is a rough fraction of the actual output current on channel n.
When you overload the output however, the channel switches into fault mode and the CSn output does something else.
- I thought I read somewhere that after a fault the CSn output assumes a voltage which is distinguishable from any valid current reading, but today I cannot find this statement anywhere in the data sheet.
- A block diagram on page 5 of the data sheet shows a switch changing the source of the CSn output from the ''Current sense'' amplifier to a block labeled ''VSenseH''.
- Table 11 on page 17 says the Sense output goes to VSenseH after a short to ground.
- Table 9 on page 12 reports that VSenseH in a fault condition lies between 7.5 and 9.5 V when RSense = 3.9k.
- The same table indicates that ISenseH in the same state is between 4.9 & 12 mA when VSense = 5 V.
- I interpret this to mean that after a fault the CSn output changes to a voltage source, in which case statement 4 trumps statement 5.
- My colleagues think that CSn stays a current source, in which case statement 4 trumps statement 5.
Does anybody know for sure? Is it somewhere in the data sheet and I just can't find it?
Thanks.
#high-side-driver-overcurrent #support