Skip to main content
Mad Max
Associate
February 23, 2018
Question

What Gate Driver is built in the STSPIN32F0 ?

  • February 23, 2018
  • 0 replies
  • 507 views
Posted on February 23, 2018 at 18:44

Hi there,

I would like to create a custom PCB build around the STSPIN32F0 MCU which integrates a gate driver and some other fancy features.

Now I need to know some specs of that driver but they're not listed in the Datasheet (or am I blind ? Maybe ...).

I need to know the resistance of the driver output for calculating if my MOSFETS will work with the driver ...

So what are the values for R_src and R_snk  ?

Next thing I would like to know: I can't find a Power rating of the driver. Only thing that's mentioned in the datasheet is the 600mW of output current (sink / source).

Can anyone help me or point me into the right direction ?

Other solutions for calculating, wether my mosfets work are also welcome.

Thank you in advance.

#gate-driver #stspin32f0 #mosfet
This topic has been closed for replies.