What causes L6472 to power up / leave reset with bridges active?
- 5 replies
- 2203 views
I have designed a board with four seemingly identical motor drivers. The four L6472 are connected to an STM32-MCU via one SPI-interface, chipselect is handled by GPIO. They share a common reset signal, also GPIO. Because of the pull-downs on /STBY_RES the L6472 will only leave reset when the MCU pulls the GPIO up.
I have verified with different boards (different production runs/board revisions) and motors that U702/U703 "Wash-Selctor Valve Driver / Dilutor Valve Driver" consistently power up or leave reset with output bridges active, resulting in high current fed into the respective motors.
On the other hand, U602/U603 "XY-S-Motor-L/R" always power up as expected - with bridges in HighZ.
I can't explain this behavior from the datasheet. Would you have any recommendations?
Thanks.