Skip to main content
This topic has been closed for replies.
Cristiana SCARAMEL
ST Employee
Sep 9, 2020 1:37 PM UTC

@Rostyslav S​ ok, than I can suggest the BLDC 65 Motor

"If you feel a post has answered your question, please click ""Accept as Solution"""

5 replies

Cristiana SCARAMEL
ST Employee
Sep 8, 2020 8:19 AM UTC

Hello @Rostyslav S​ 

The EVSPIN32F0251S1 is able to drive three-phase permanent magnet synchronous motors (PMSMs) and brushless DC (BLDC) motors with compatible voltage and current ratings (see details below).

The board is a 3-phase complete inverter based on the STSPIN32F0251 controller, which embeds a 3‑phase 250 V gate driver and a Cortex®‑M0 STM32 MCU.

The power stage features STD17NF25 MOSFETs, but can be populated with any IGBT or Power MOSFET in DPAK or powerFLAT 6x5 package.

The board has a single-shunt sensing topology, and both the field-oriented control (FOC) and sensored or sensorless 6‑step control can be implemented.

With the mounted components the maximum ratings of the board are the following:

  • Power stage supply voltage from 15 VAC (20 VDC) to 120 VAC (170 VDC)
  • Overcurrent protection set to 16 Apeak.
"If you feel a post has answered your question, please click ""Accept as Solution"""
Rostyslav S
Associate II
Sep 8, 2020 9:25 AM UTC

Thank you, Cristiana. This information is already provided in board manual.

Actually I was looking for motor part numbers that were tested with this board.

The motor I am currently using matches above requirements (except rated power, so I have upgraded EVSPIN32F0251S1 to support 500W motors), but I am not able to start it spinning. So I am looking for a motor that was specifically tested with this board and it 100% works.

Cristiana SCARAMEL
ST Employee
Sep 9, 2020 12:37 PM UTC

Hi @Rostyslav S (Community Member)​ are you targeting a sensored or sensorless application?

"If you feel a post has answered your question, please click ""Accept as Solution"""