Question
What are the "STM32-based control board"?
In the manual of STEVAL-IPM08B I read:
"The STEVAL-IPM08B is compatible with ST's STM32-based control board, enabling designers to build a complete platform for motor control."
I wonder what are these "STM32-based control board" that are compatible with the signal connector.
By the way, in the same document I read:
"Motor control connector (32 pins) interfacing with ST MCU boards"
but in the schematic that connector has 34 pins....