What am I doing wrong with the l6470 stepper driver?
We develop electronics for controlling multiple stepper motors and use the L6470 as drivers. Radiators with fan cooling mounted on the chip of the driver (above). The current does not exceed 2 amperes. Radiators remain cold.
The problem is that drivers after working on hold for about 40 minutes seem to overheat and degrade. The overheat warning flags appear immediately before the overheat shutdown.
After the driver shutdoun it loads the SPI and all drivers on the bus stop responding.
Once an overheated driver starts to shut down after a few minutes or seconds of operation, even without a connected motor.
What could be the problem? Maybe I have to cool the drivers only from the bottom?
Thanks