Skip to main content
SA.9
Visitor II
December 26, 2020
Question

We have to design programmable power supply as per below spec 1. Vin: 230VAC, 50Hz 2. Vout: 0-120VDC or 20-120VDC, 12A max (variable with external control voltage from 0 to 5V) 3. Temp: -20 to +55 C Please suggest us any part number.

  • December 26, 2020
  • 0 replies
  • 428 views

Hi,

We have to design programmable power supply as per below spec

1. Vin: 230VAC, 50Hz

2. Vout: 0-120VDC or 20-120VDC, 12A max (variable with external control voltage from 0 to 5V)

3. Temp: -20 to +55 C

Please suggest us any part number, this is for Ground based application. Is SG2525 is suitable? If so please suggest any reference design

This topic has been closed for replies.