Skip to main content
SDwiv.2
Visitor II
May 15, 2020
Question

We are using STC3117 Fuel Gauge. Can we read a configured RAM data from one device and write the same RAM data to another device and if yes how??

  • May 15, 2020
  • 0 replies
  • 524 views

We are using STC3117, and we are performing a charge and discharge cycle to avoid any battery fluctuation issue so if we need to do it with mass number of device, it is not possible to perform same task so can we perform this in a device and get RAM of this device and write same data to another device. Is it possible if yes then how we can do that and will it work for all devices.??

This topic has been closed for replies.