Skip to main content
Associate II
September 24, 2025
Question

VNH5019A-E circuit diagram configuration

Hello, I am designing a circuit using VNH5019A-E motor driver.
Is there a problem if the capacitor is installed on the motor output pins OUTA and B? The value is about 10uF.

For example, the charging and discharging of the capacitor leads to situations where low speeds such as PWM 10% and 20% cannot be controlled.

Is it possible to not use capacitors for the output? If possible, to what extent is it possible? This is to remove the noise from the EMC/EMI test.

 

Additionally, is it correct that this motor driver can't use PWM 100% because it has H bridge structure? Because it requires switching of high side and low side FET? If so, if I set it to 100% and give the PWM signal, does it operate at 99%?? Or does it operate incompletely? For example, it generates noise..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
September 24, 2025

Are you sure you mean the VNH5019A-E?

The VNH5019A-E is an H-bridge motor driver that drives a motor directly via OUTA and OUTB – why do you think you need a capacitor for that?

The motor driver can do 100% PWM because it does not need boost capacitors on the half-bridges.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.