Skip to main content
Associate II
August 8, 2025
Question

VN9E30F Channel deatils

 

VN9E30FTR – 6-channel high-side driver with 24-bit SPI interface

Max. DC output current is internally limited to 35A for channels IOUT0, IOUT1, IOUT2, IOUT3, IOUT4, and IOUT5

  1. Whether this 35A limit is shared across all channels or applies individually to each channel.
  2. What is the maximum current for each channel
  3. Conditions applicable when switching the load per channel.
  4. Can we parallel 2 or 3 channels to get single output.
  5. If we are not using any channel cant it be disabled / floated ( Is SOCR used for Enabling / disabling the channel )
This topic has been closed for replies.

1 reply

ST Employee
August 11, 2025

Hello @KumarTP,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Best regards,
Maxime

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.