Skip to main content
Explorer
January 7, 2025
Solved

VN9D5D20FN operating with Vcc 5v

Hello,

We are looking to use VN9D5D20FN (SPI management and monitoring) as power distribution solution for our product. There are 4 channels which are fed from common output of a buck converter. The buck has 5V 3.2A max output and that goes into VN9D5D20FN, to be shared across 4 channels.

VN9D5D20FN datasheet specify minimum operating voltage 4V with a recommended operating voltage of 13V. At 5V  we are very close to this min threshold, any considerations?

Thanks.

 

Cio

This topic has been closed for replies.
MHoll.2
MHoll.2Best answer
Senior III
January 7, 2025

Hi,

I don't think that 5V is a problem (the undervoltage shutdown limit is 2.7V max.).

You only have to deal with a sightly higher Rds ON (CH 0,1: max. 12.3mOhm, CH2,3: max. 37mOhm  @ 4V, 25°C)

Martin

1 reply

MHoll.2
MHoll.2Best answer
Senior III
January 7, 2025

Hi,

I don't think that 5V is a problem (the undervoltage shutdown limit is 2.7V max.).

You only have to deal with a sightly higher Rds ON (CH 0,1: max. 12.3mOhm, CH2,3: max. 37mOhm  @ 4V, 25°C)

Martin