Skip to main content
igamoso
Associate III
Dec 8, 2022 5:57 AM UTC
Question

VN750PTTR-E Date Code

Dear Support,

Please confirm if the DC for the part number VN750PTTR-E in the marking "235" is 2235.

Year: 2022 and Week 35.

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Dec 8, 2022 8:32 PM UTC

    The date codes are to be interpreted as always: YWW, which also applies to the VN750PTTR-E, which has the component marking VN750 and the line below with PT.

    Since VN750PTTR-E was launched in 2004, the examples should be read as:

    • 235 = 2012 or 2022, week35

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.