Skip to main content
AAdin.1
Associate II
July 10, 2024
Question

VIPER26LD 310VDC to 15VDC Converter Design Issue

Hi, 

I have used following STM reference design for the buck converter. When I power the circuit output doesn't stabilize. What am I missing?

 

This is from. STEVAL-IHM023V3

Screenshot 2024-07-10 at 16.18.33.png

Here is my design.

 

Screenshot 2024-07-10 at 16.19.08.png

Here is the layout

 

Screenshot 2024-07-10 at 16.20.17.png

Best Regards.

This topic has been closed for replies.

5 replies

Peter BENSCH
ST Technical Moderator
July 10, 2024

> When I power the circuit output doesn't stabilize.

What does it mean?

What is your load?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AAdin.1
AAdin.1Author
Associate II
July 10, 2024

Output rises and collapses. There is no active load at startup state, when I supply 15V with my bench power supply output circuit draws 0.025Amps.

 

Best regards.

Peter BENSCH
ST Technical Moderator
July 10, 2024

The buck regulator must have a sufficient load, 50...100mA should always flow as a minimum.

Where have you connected the 15V - at the input of this regulator, which requires an AC of at least 80V at the input, which corresponds to about 110V peak voltage?

What is the saturation current of your inductor L2 and what the expected output current?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Peter BENSCH
ST Technical Moderator
July 10, 2024

Yes, I recommend a dummy load and also a test with a normal input voltage, possibly with an isolating transformer for safety reasons. Then you can also view the output signal with a scope.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.