Skip to main content
Associate
January 23, 2025
Solved

VIPER26K device fails when we tried to measure VDD pin voltage with respect to power ground

We designed a buck converter with (300-800) input DC voltage and the output voltage is 24V.  The max load current is 150mA.  We noticed two issues here:

1. The device fails when we try to measure VDD pin voltage with reference to Power Ground (DC input ground).  Though the VDD voltage is with reference to device ground (pins 1,2,3,4,6), but why it should fail when we use power ground as a reference with a Digital Multimeter.  This has happened thrice and in all the cases, the device failed silently (no sounds, no physical damage etc.,).  All this happened at 150V DC input voltage itself.

2. In the second case, the device failed at 800V DC input when we tried to connect 100mA resistive load.  No probe is connected anywhere in the circuit.  However, we used the same compensation network as given in ST AN 5380 (15V, 1.5W buck converter and could not arrive at the values for 24V output voltage.  If the compensation network is a problem, can someone please help us in arriving at the correct values for compensation circuit.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 23, 2025

Welcome @NSRPrasad, to the commnunity!

Please share your schematics you are testing.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 23, 2025

Welcome @NSRPrasad, to the commnunity!

Please share your schematics you are testing.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NSRPrasadAuthor
Associate
January 24, 2025

Many thanks and nice to get in touch with you Peter.  Enclosed the schematic & layout files here. Device fails with or without ZD1 Zener.  There was no load at the output when we tried to probe the VDD point with ref. to DC INPUT negative.

Please refer to bottom right-side section for the power supply part layout and traces. 

Best Regards and Many thanks once again