Question
Viper26k buck converter has an unstable output.
- 8 replies
- 2100 views
We designed a buck converter based on AN5380 with an input of 600Vdc and an output of 12Vdc.
The device turns on at around 55Vdc, but the output keeps shutting itself off and turning on again (image1). This keeps happening as we turn up the voltage. However, at around 80Vdc, the output changes to many small bursts and then a large spike up to 12Vdc (image 2). Is this only a problem that appears with lower voltages?
Attached is the schematic of the circuit (image 3). Are the values we chose unsuitable for this application?