Skip to main content
Associate III
June 3, 2024
Question

Viper115 cannot produce the required current

I am designing a new SMPS for my project I need 350mA at 15V but I could not get more than 100ma. when I reach to 100mA output voltage was start to decrease. when current goes to 200mA, output is like a sinusodial signal from 9v to 15V. I design my SMPS with E-design suit but its not working stable. I need urgent help

 

Mnemonic_0-1717402436350.png

 

This topic has been closed for replies.

11 replies

Peter BENSCH
ST Technical Moderator
June 3, 2024

What are the parameters of the coil L, particularly the saturation current, that you used with 330µH?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MnemonicAuthor
Associate III
June 3, 2024

Hi Peter,

thanks for your fast reply. you can find parameter of coil at below and also I share its dataheet link

https://cdn.ozdisan.com/ETicaret_Dosya/527916_8583741.pdf

 

 

Mnemonic_1-1717408357806.png

 

Peter BENSCH
ST Technical Moderator
June 3, 2024

For this type of coil, the manufacturer Core Master has only specified the DC current, but no saturation current, so that I cannot recommend such a coil for DCDC converters with your parameters. In addition, due to the small dimensions of the coil, only thin wire is used, which results in a very high DC resistance of 1.26 Ohm.

Please get a coil with a saturation current of at least 1A.

In addition, the output power is at the upper limit of the VIPER115HS. At full load, I calculate a junction temperature of approx. 124°C, so you might want to consider a larger VIPER.

Another question: your values for Rc, Cc and Cp lead to a low phase margin, so there may also be a stability problem. For your basic values, I calculate values of 150k, 7.5nF, 100pF instead of your 1k+100nF+10nF.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MnemonicAuthor
Associate III
June 3, 2024

Thanks for your reply,

I will try your suggest. Also could you explain function of Comp pin ?

how could you calculate that values

MnemonicAuthor
Associate III
June 3, 2024

Hi again,

I have this coil. I was try with this but nothing was changed. Do you have any opinion for this

 

https://eu.mouser.com/ProductDetail/Bourns/SRN1060-471M?qs=UvjENeDOEefs7qNqJQPBYw%3D%3D

Peter BENSCH
ST Technical Moderator
June 3, 2024

The new coil has a saturation current of 900mA, which might just be enough, but the DC resistance is not much better at 0.95 ohms. The inductance is with 470µH also somewhat high, which would have to be checked again with the eDesignSuite. Nevertheless, you should be able to continue working with this coil for the time being.

Pin COMP:

As mentioned in the datasheet, the compensation network is to achieve stability and good dynamic performance of the control loop. Since it is not trivial to calculate it if you are inexperienced, you should use the values of the eDesignSuite for your environment parameters.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MnemonicAuthor
Associate III
June 3, 2024

Ok thanks alot for your information.

could you suggest a coil to me which is best for us ?

Peter BENSCH
ST Technical Moderator
June 3, 2024

As already mentioned, it should work with the coil from Bourns if you change the  compensation network as suggested by the eDesignSuite.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Super User
June 3, 2024

the design, buck, non iso, 15V , 400mA :

AScha3_0-1717422242063.png

coil: 

AScha3_1-1717422314706.png

Why not using 1,6A coil, as recommended by eDesignSuite ? (and other parts/values also...)

If you feel a post has answered your question, please click on " Best Answer ".
MnemonicAuthor
Associate III
June 10, 2024

Hi @Peter BENSCH 

I was changed my topology to Viper222XS because of your heat suggestion. But I have same problem with new IC

I was built my project with belowed shema but when its going to shutdown when current is going to 400mA. My circuit is start with 100mA but when pust to start button its going to 400mA immidiatly ( its like inrush current) and Viper will going to shutdown and start again 1Sn later

 

is there anywhy to disable over current protection ? 

Just I could not find 1.2mH coil and I was used 1mH coil with belowed datasheet

 

https://cdn.ozdisan.com/ETicaret_Dosya/514828_7988607.pdf

 

Mnemonic_0-1718010206237.png

Mnemonic_2-1718010573965.png

 

 

Mnemonic_1-1718010530865.png

 

 

MnemonicAuthor
Associate III
June 11, 2024

Can anyone help about this problem

@AScha.3 @Peter BENSCH