Viper06 Buck mode converter, and AN4260
- 3 replies
- 2458 views
Hello, I need to be able to generate a small DC voltage from an AC voltage.
The App Note 4260 looked absolutely perfect - exactly what I needed - 12V 150mA buck converter. Simple. no flyback transformers, etc. But I was a bit confused as to the GND connection on the IC. It looks like it is connecting to the V-Out instead, with a diode to gnd.
So i went into the edesign suite and used the exact same parameters. the design it shows before you hit "Start design" also shows the diode to gnd on the GND pin, but it also shows another ground symbol. Can you clarify the two different grounds?
The other thing I noticed - it shows a bridge rectifier on the AC input before you tap "start design", but the app note and design you see after you tap "start design" just show the simple single diode rectifier. Can you clarify if I need to add a bridge rectifier on the front? Do I also need the other diode then?