Skip to main content
Associate III
June 14, 2024
Question

Viper comp design

Hello everybody,

I need to user Viper115HS or Viper222XS vith 15V 600mA output at non isolated buck topology. I was designed my Fb pin with 130K Ohm and 11K Ohm resistors. But I can not find right Comp pin configuration. could you write capasitor and resistor configuraton for 15V 600mA output

This topic has been closed for replies.

3 replies

AScha.3
Super User
June 14, 2024

Hi,

always same questions...?

1. you could use, what eDesign suite telling :  (for 400mA max.)

AScha3_0-1718348934969.png

2. 600mA not possible with non-iso buck ; 590mA would be absolute maximum. But "critical" design.

3. Use a transformer (as almost everybody...) and it will work . (If you have the matching transformer ! )

If you feel a post has answered your question, please click on " Best Answer ".
MnemonicAuthor
Associate III
June 14, 2024

I can not calculate for 590mA at e-design. could you share

AScha.3
Super User
June 14, 2024

Me too.. just maximum possible message there. Not yet calculation.

 

 

If you feel a post has answered your question, please click on " Best Answer ".