Question
Viper 16 hangs up
Posted on May 09, 2013 at 10:12
I put in a technical support request on this but no response.
I'm running a Viper16 in a simple non-isolated buck configuration as per the data sheet. There is a spark ignitor on the board and sometimes when the spark occurs, the Viper16 shuts down. I can understand it might go into one of its overload conditions but it does not recover. Vdd sits at 12V, 0.25V on FB and 0V on LIM and COMP. If I inject current into Vdd, the Viper16 starts again. Strange. Has anyone had this sort of problem with the Viper16 or other Viper chips?