Skip to main content
dvelasco
Associate II
February 11, 2015
Question

Using X-NUCLEO-IHM01A1 without an STM32 Nucleo board

  • February 11, 2015
  • 0 replies
  • 466 views
Posted on February 11, 2015 at 22:42

I'm trying to use an X-NUCLEO-IHM01A1, but without an STM32 board. That is, I need to wire up each of the necessary pins individually, sending the proper signals via another microcontroller.

For now, I just need to get to the point at which the board powers up and the green D7 LED comes on.  What steps do I need to perform?  I applied 3.3V to the IOREF pin on CN6 and I tied the the /RST pin on CN5 to 3.3V.  Are these steps correct, and what else do I need to do?
This topic has been closed for replies.