Skip to main content
Gaston
Associate III
May 5, 2021 8:02 AM UTC
Solved

Using STEF01 as a high-side switch

Hi,

I'm planning to use STEF01 as a high-side switch plus an external MOSFET for blocking inverse current from load. Is this feasible or I would be wrong?

gaston

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 5, 2021 3:11 PM UTC

If you need more than 2.4A (until then the IPS160HF would be the better solution, also because it is considerably faster) and you are satisfied with the switch-on time (min 3ms), this should be possible. However, keep an eye to the maximum input voltage.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 5, 2021 3:11 PM UTC

If you need more than 2.4A (until then the IPS160HF would be the better solution, also because it is considerably faster) and you are satisfied with the switch-on time (min 3ms), this should be possible. However, keep an eye to the maximum input voltage.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Gaston
GastonAuthor
Associate III
May 5, 2021 3:27 PM UTC

Hi Peter,

Understood. The problem is IPS160HF does not have the option for Reverse Current Blocking.

I'm basically looking for an alternative part to MP5016H but in my application the switching times are not so critical. I think STEF01 can be a good one. Thanks!

regards,

gaston