Skip to main content
jchristensen
Visitor II
February 11, 2010
Question

Using 3.3 volt logic with the VNH3SP30-E

  • February 11, 2010
  • 1 reply
  • 600 views
Posted on February 11, 2010 at 18:04

Using 3.3 volt logic with the VNH3SP30-E

This topic has been closed for replies.

1 reply

muratterzi2
Associate
May 17, 2011
Posted on May 17, 2011 at 10:19

in order to get a stable data flow and handshaking between processor and vhn3sp30 You ust use 74lvc244 at the output of processor . This logic has 5 v tolerant 3.3v compatible structure. And then you must connect 74hct244 at the output of 74lvc244 to shift 3.3v logic to 5 volt. This is true only for data flow from processor to your device. in case data flow from device to processor needles to use 74hct244.