Skip to main content
luke23
Associate III
March 24, 2014
Question

Use of an NTC temperature feedback device (non-semiconductor junction)

  • March 24, 2014
  • 1 reply
  • 494 views
Posted on March 24, 2014 at 02:53

Hi

The MC Toolbox wizard (and presumeably the MC library itself) seems to support only the use of p-n junction temperature feedback devices (25mV/degC), with support to alter coefficients.

In our application we are using an NTC thermistor.  Any plans to support these additional devices, please?  Simple parametric would be required to specify the temperature transfer function to the library.

Thanks

Luke

#ntc-temperature-diode
This topic has been closed for replies.

1 reply

Gigi
ST Employee
March 31, 2014
Posted on March 31, 2014 at 09:48

Yes, we plan to extend the support also for negative slope and maybe for other kind of transfer functions.

Ciao

Gigi