Skip to main content
Associate
May 27, 2025
Question

USB PD and Data transmission from two DFP ports to one UFP

I want to design a USB4 Hub where one UFP USB C port has data connection and charging capabilities for a DFP, but can also get charge from a STUSB4710 that I'll supply with a DC voltage externally. So my hub would have a DC input and a USB C data I/O with DFP charging.

I'm fairly new to USB C design so I don't really know how I can manage CC from both the STUSB4710 and from the DFP USB C for simultaneous UFP charging and data transmission.

Any help would be appreciated.

This topic has been closed for replies.

4 replies

Peter BENSCH
ST Technical Moderator
May 27, 2025

Welcome @Ashtraywasp, to the community!

The CC lines of USB-C PD (UCPD for short) have nothing to do with the data lines. In your case, the former are managed by the STUSB4710.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
May 27, 2025

Thanks! I did consider that but I thought that the data port would need the CC lines for orientation detection, so unless I'm mistaken it'd need CC from the STUSB for PD negotiation and from the data port for orientation detection, and use something that can mux between the ports?

Peter BENSCH
ST Technical Moderator
May 27, 2025

Correct.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.