Visitor II
October 17, 2022
Question
Unable to detect stall condition of stepper motor using powerSTEP01 Voltage Mode
- 3 replies
- 3227 views
Currently we are evaluating voltage mode feature of powerstep01
Motor Parameters:
Motor Phase Resistance: 8.4 ohm
Motor Phase Inductance: 5.2 mH
Ke: 0.07392
We have tested voltage mode by changing current from 0.5 to 1.1 A. Test report are attached
Also In application we are operating motor from 2 to 14 RPM
Kindly share your feedback on test result and test procedure.Please go through it. Let me know anything is required.