Skip to main content
PG.6
Associate
July 19, 2021
Question

TSM1012

  • July 19, 2021
  • 9 replies
  • 3600 views

Hai,

I wanted to make a battery charger using non isolated boost IC. I came across this TSM Voltage and current controller IC. But this IC has been only used in insolated application. Is it possible to use this IC in non isolated converter. I will attach the block diagram of the same.

This topic has been closed for replies.

9 replies

Peter BENSCH
ST Technical Moderator
July 19, 2021

Welcome, @Community member G​, to the community!

You should be able to use the TSM1012 in a non-isolated project, as long as the boost IC is controlled by a pulldown similar to an optocoupler.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PG.6
PG.6Author
Associate
July 19, 2021

Hello Peter,

Thank you for the quick reply. Is it okay if i use an opto-coupler for feedback in an non-isolated converter along with TMS IC. Will this be able to charge Li- Ion battery?

Regards,

Praveen Kumar G

Peter BENSCH
ST Technical Moderator
July 19, 2021

Yes, you can do it with an opto-coupler, but that's wasted money.

As I said - TSM1012 could drive the boost IC directly if this boost IC can be controlled by a transistor of an optocoupler. The TSM1012 contains a pull-down structure, which is very similar to that transistor.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.