Skip to main content
NPAL.1
Visitor II
May 4, 2023
Question

TS33 datasheet mentions that it supports 1.8V fixed output voltage too, but cannot find relevant ordering code.

..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
May 4, 2023

Welcome, @NPAL.1​, to the community!

Unfortunately, the first overview page of the data sheet indicates voltages that are not currently supported. However, the information is relevant in the data sheet, section 7 (Ordering Information):

  • 1.25V
  • 2.048V
  • 2.5V
  • 3.0V
  • 3.3V

That means, 1.8V, 4.096V and 5V are not (yet) available.

And if you want to ask now when this will be the case - that is currently unpredictable.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.