Skip to main content
Christian Landry
Associate
March 20, 2017
Question

Terminal Emulator COMM and X-CUBE SPN11

  • March 20, 2017
  • 1 reply
  • 796 views
Posted on March 20, 2017 at 20:21

Trying to communicate to a X-Nucleo IHM11M1 demo board and the Nucleo-F401RE using Tera Term and the IHM11M1 does NOT respond to sent commands.  I am running the X-Cube-SPN11 software sucessfully by uploading it to the IHM11M1.  I can manually start the BLDC motor using the on-board buttons on the -F401RE board.  When I start the terminal emulator SW to communicate to the IHM11M1/F401RE demo boards, I get no response from the demo boards.  NOTE, when I press the reset button on the F401RE, the menu screen apprears in the terminal emulator window as shown below: 

*******************************************************************************

*             X-NUCLEO-IHM11M1 - 6-Step Motor Control Expansion board        *

*******************************************************************************

 List of commands:

  <STARTM> -- Start Motor

  <STOPMT> -- Stop Motor

  <DIRECT> -- Set the Motor direction CW or CCW

  <SETSPD> -- Set the Motor Speed

  <GETSPD> -- Get the Motor Speed

  <STATUS> -- Get the Status of system

  <POTENZ> -- Enable/Disable the potentiometer

  <HELP>   -- Show the help menu

             ************* MAIN MOTOR PARAMETERS ***************

  <INIREF> -- Start-up duty cycle

  <ACCELE> -- Motor acceleration value during startup

  <POLESP> -- Set the Motor pole pairs

          ****** PI REGULATOR PARAMETERS - SPEED LOOP  ******

  <KP-PRM> -- Set the PI proportional term

  <KI-PRM> -- Set the PI integral term

However, when I try to send any of the commands above I get no response.  Is there a special character required when transmitting the commands?  Do I need another driver to communicate to the  demo boards while the motor is running?  I am following the quick start guide to get this up and running.

I am using IAR to compile the code

0690X00000606ToQAI.png

#x-cube-spn11 #ihm11m1 #f401re
This topic has been closed for replies.

1 reply

Christian Landry
Associate
March 23, 2017
Posted on March 23, 2017 at 20:55

I've learned one thing since this post. 

1. To enter a command, just type the command with no arguments. A prompt will appear where you can input the parameter. Obviously, the coder of the interface was kind enough to not provide instructions.