Temperature threshold raised
Hi,
Using SPINFamily Evaluation Tool 3.2, STnucleo-f401re and IHM03A1, I try to drive a 48V-9A motor.
On IHM03A1, I add 15mOhm/3W resistances in parallel of R1 and R2, so R1 and R2 value is now 13mOhm.
In SPINFamily interface, I choosed current mode, set run current to 7,2A (93,75mV) and overcurrent threshold to 8,41A (218,75mV).
I successfully start to run the motor at constant speed but after several minutes (around 3minutes), temperature threshold is reached and board stop, do you know why ?
Measured output current is 6A.
Thanks