TD350E - interpreting date/batch codes and desaturation sensitivity
I'm presently debugging an intermittent desaturation issue in a stable product platform (stable as in 10+ thousand units over more than a decade).
From what I can tell so far the TD350 device is signalling a desat on occasion without a reason I can observe (it is strangely episodic also)
I'm still working on it, but it appears that the date/batch code has changed between problematic and non-problematic setups....
Two questions
1)How do interpret the date code written on the device?
some items have KPB0909 and others MZMF909 written on them.
2) Where can I find some elaboration on the desaturation detection timing.
exactly how fast is the comparator in the TD350 that compares the incoming voltage against the internal reference at about 7V? I have reviewed both datasheet and application note?
thanks in advance.
Scott