Skip to main content
Explorer
November 25, 2023
Solved

TCPP03-M20 using Mosfet driver outputs for logic control

Hello,

I'm using TCPP03 for a DRP solution. For my design it would be good to use the Mosfet drivers for controlling a logic input for further power control instead of using Mosfets. Is it possible to use the gatedrivers with the SRC-pins connected to Ground and feed the GATE-Pins to an input of a logic device? I'm aware that I have to take care for the logic level translation.

I did already tests and it worked so far. Just to get safe that there will be nor furhter impacts, I want to know your suggestion for this.

Regards

Michael Houzer

 

 

 

This topic has been closed for replies.
MROUV.1
MROUV.1Best answer
ST Employee
November 27, 2023

Hello Michael,

 

Your case is clear and TCPP03-M20 match to your needs.

 

To rephrase, TCPP03-M20 SOURCE and SINK gate drivers must drive logical levels.

SOURCES are connected to the GND.

GATES (5.0V output voltage) can be connected to :

  • 5V HZ input
  • 3.3V HZ input with rail-to-rail structure that let the gate driver current flows (<50µA)
  • 3.3V HZ input FT
  • 3.3V HZ input with 3.3V Zener to limit voltage that let the gate driver current flows (<50µA)

 

There is no TCPP03-M20 restriction for this case.

 

Best regards,

Mathieu

1 reply

MROUV.1
MROUV.1Best answer
ST Employee
November 27, 2023

Hello Michael,

 

Your case is clear and TCPP03-M20 match to your needs.

 

To rephrase, TCPP03-M20 SOURCE and SINK gate drivers must drive logical levels.

SOURCES are connected to the GND.

GATES (5.0V output voltage) can be connected to :

  • 5V HZ input
  • 3.3V HZ input with rail-to-rail structure that let the gate driver current flows (<50µA)
  • 3.3V HZ input FT
  • 3.3V HZ input with 3.3V Zener to limit voltage that let the gate driver current flows (<50µA)

 

There is no TCPP03-M20 restriction for this case.

 

Best regards,

Mathieu