Skip to main content
RMas
Associate II
Jan 5, 2023 10:43 AM UTC
Question

TCPP01-M12 FLT fault indicator

I'd like to add an LED indicator to the FLT pin so it sinks current when it becomes active low. The LED anaode would be tide high with a resistor in series. The spec sheet says this pin has a resistance of 250Ohms when active. How much current can this pin sink and is approach a suitable way to achieve this?

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
Jan 5, 2023 12:26 PM UTC

As you will have seen, the maximum current in pin FLT/ is not specified in the data sheet.

However, since this is a logic output that is normally working on a pull-up of 10k, you can probably assume an applicable current of 1mA, which is a bit low for most LEDs. Therefore, it maybe makes sense to drive the LED with an amplifier, e.g. a single-gate logic gate, a pnp BJT or a logic level p-channel FET.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.