Skip to main content
Associate II
December 19, 2024
Question

STWLC38 GPIO Functions

Can you help to explain the function of these GPIO settings on the RX IC?

0x0A - RX power Out OD - this function is not mentioned in the datasheet or EVK user guide but is available through the GUI. How does it work?

0x05 - what does FW ready indicate? Is it related to Vout turn on? Is this a Push Pull or Open Drain pin?

0x29 and 0x2A - What is the function here? Does this pin act based on any information on the IC, or does it just stay high/low?

This topic has been closed for replies.

2 replies

ST Technical Moderator
December 20, 2024

Hi Sir

 

GPIO_FUNC_RX_PWR_OUT_OD = 0x0A,            #///< 0A - out_od: Power output enabled (0=on, 1=off)
when vout is turn on, this gpio will be open drain output high
 
GPIO_FUNC_FW_RDY = 5,                   #///< 05 - out_pp: High on FW ready (before main loop)
0x05 - what does FW ready indicate? -- when rx is power on and fw feady, this is push pull high
 
GPIO_FUNC_OD_LO = 0x29,                    #///< 29 - out_od: driven low
GPIO_FUNC_OD_HI = 0x2A,                    #///< 2A - out_od: driven high
GPIO_FUNC_PP_LO = 0x2B,                    #///< 2B - out_pp: driven low
GPIO_FUNC_PP_HI = 0x2C,                    #///< 2C - out_pp: driven high
 

about wlc38 gpio control please refer this link for more infor

https://github.com/STwirelesscharger/Python_FT260_ST_WLC/blob/main/wlc38_register.py

https://github.com/STwirelesscharger/Python_FT260_ST_WLC/blob/main/a8_wlc38_gpio_control.py

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
pEEterAuthor
Associate II
December 20, 2024

Thank you!