Skip to main content
Associate II
September 3, 2024
Question

STWLC38 FOD tuning BPP and EPP configuration

Hello, I have some questions regarding a problem with a BPP receiver I am designing. After performing tuning, the FOD configuration on the STWLC38 works well with BPP chargers, but some EPP chargers will trip FOD when the receiver is placed.

Is it possible to use two different FOD configurations on the STWLC38 for BPP and EPP even if the STWLC38 is configured as a BPP receiver?

Is it possible to change the STWLC38 FOD parameters by sending I2C messages without needing to reprogram the RX?

If the above two are not possible, is it possible to implement this with custom firmware?

Thank you!

This topic has been closed for replies.

1 reply

ST Technical Moderator
September 30, 2024

Hi

There are bpp and epp fod in the default settings.

also fod register start with 0x00B6, and struct as blow picture, you can read and test it.

willzhou_0-1727658589669.png

willzhou_1-1727658896995.png

 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.